11 Revision History
Changes from Revision B (July 2022) to Revision C (May 2023)
- Fixed J23 pin 11 to correctly reflect 3.3V
connectionGo
- Added J26 to the table of pin connectionsGo
- Clarified the pulse length of trigger output 2 as 19.4
μsGo
- Corrected that trigger input 1 advances to the next pattern waiting
for a trigger inputGo
- Added information regarding supported GUI and firmware versions for
the DLP5500 DMDGo
- Added descriptions of items in DLPC900REF-SWGo
- Added DLPA200 fault to the list of descriptions of status indicatorsGo
- Added information about the DLPA200 fault conditionsGo
- Added information that the Get command only reads values from the
primary controllerGo
- Added note that the EVM is connected only on Pixel Clock
1Go
- Added link to table in DLPC900 Programmer's Guide of minimum exposure timesGo
- Added a note to the Caution statement regarding supported GUI and
firmware versions for the DLP5500 DMDGo
- Added information about the number of patterns the EVM can hold in
flash memoryGo
- Added information to the caution note about the recommended firmware
versionGo
- Added new section to describe how to reprogram firmware to support a different
DMDGo
- Updated Figure 7-23
changing Cypress to InfineonGo
- Added section describing how to program an EDIDGo
- Added pin J18 table and
description Go
- Created new section for pin J26Go
- Changed minimum current from 0 A to 5 AGo
- Added information about J18 matching connectorGo
Changes from Revision A (April 2022) to Revision B (July
2022)
- Changed all instances of legacy terminology to "Primary" and
"Secondary" throughout this guide.Go
- Added Note: Heartbeat is present even if no DMD is present.Go
- Changed J11 "HOLDBoot" jumper description to "BOOTHold" jumper.Go
- Added Controller Board and DMD Board Assembly
instructions.Go
- Updated to Secondary terminology for Secondary Present and Ready Status item.Go