Creating a Video Pattern Mode sequence is
also similar to Pattern On-The-Fly Mode. The difference is that the patterns
are streamed from the input video source. The user must create the video images and
then input them through the RGB parallel interface. The input video source vertical
sync is used as the triggering mechanism. The input video source must be stable and
locked and continuously being applied, otherwise the firmware detects that the
source was lost and a solid curtain is displayed. While the video source is stable
and locked, the status box for Locked to External Source remains checked.
Follow these steps to create a Video Pattern Mode sequence.
- Make sure the EVM is powered up and operating correctly, and the Connected radio-button is lit green.
- Select Video Mode from the Operating Mode group box, and then
select the HDMI radio-button from the IT6535 Receiver group box
and finally click the Set button. (Select the DisplayPort
radio-button if using this input connector). The Locked to External
Source status box is checked after a few seconds.
- Verify the video source is displayed. If no video source is displayed, then
make sure the PC or host is supplying the correct resolution and frame rate. See
Video Support for video support.
- Select Video Pattern Mode from the Operating Mode group box, and then click the Pattern Design button so that the large black panel is displayed as shown in Figure 7-6.
- Click the Add Pattern button on the Menu bar and add 3 patterns.
[Hover over buttons in the Menu bar to see their tool tip]
- Click the Select All Patterns button to select all images.
- Set exposure time to 1215 µs and dark time to 0 µs.
- Select the first image and select a bit depth of 2, start bit G0, and color Green.
- Select the second image and select a bit depth of 4, start bit R0, and color Red.
- Select the third image and select a bit depth of 3, start bit B0, and color Blue
- Click the Select All Patterns button.
- Remove the check from the Frame Change box.
- Select pattern 0 (first pattern) only and check the Frame Change
box.
- Click the Update LUT button.
- Click the Start button to run the sequence. The system displays a green
2-bit sequence based on G0 - G1 for 1215 μs, a red 4-bit sequence based on R0 -
R3 for 1215 μs, and a blue 3-bit sequence based on B0 - B2 for 1215 μs with the
remainder of the video frame time dark. This sequence repeats every frame with
the new video data for that frame.
- Click the Stop button to end this example.
See Figure 7-14 after all settings have been applied.