DLPU101C december 2020 – may 2023 DLPC900
Click the Batch Files button at the top of the GUI to display the Batch Command Sequence panel as shown in Figure 7-17. If the Enable Command Logging box is checked, the panel displays all the commands the user clicks on the GUI. When clicking the Save Batch File button, the content that is in the panel is saved to a text file containing the command descriptor followed by the command data. This batch file can then be reloaded at a later time using the Load Batch File button and executed or it can be added to the firmware to be executed using the Batch files Stored in the EVM group box. This group box lists all the batch files currently in the firmware.