To reprogram the firmware to support a different DMD, perform the following:
- Place the boot hold jumper onto the EVM.
- Power up the EVM. Upon power up, the default DMD in the GUI is the DLP6500.
- Select the new target device from the GUI menu.
- In the Firmware tab, click the Browse button.
Search for the firmware in the Texas
Instruments-DLP\ directory that matches the target
DMD. For the single controller EVM this is either
the DLPLCR65EVM or the DLPLCR55EVM. Choose either
the OOB image or a custom firmware that matches
the target device.
- Click the Upload button and wait for the process to complete.
- Power down the EVM and remove the boot hold jumper.
- Attach the new hardware and power on the EVM.