DLPU101C december 2020 – may 2023 DLPC900
The Status panel indicators show the current state of the DLPC900. When any of the boxes are checked, this indicates the stated text has occurred. Any boxes that state an error and remain checked must be corrected before continuing to operate the EVM.
The following is a description of each status indicator:
DLPA200 Fault – The box is checked whenever a DLPA200 fault has occurred. The box is active when a DLP5500 DMD is connected.