SPRAD21E May 2023 – February 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM62P-Q1
Refer to the note regarding shared IO pins in Device Comparison section of the device-specific data sheet. IOSETs are a collation (grouping) of signals specific to an interface that are timed as a set. The processor is timing closed using IOSETs. Any interface that has IOSETs must select all interface signals from the same IOSET. Some interface signals may be shared over multiple IOSETs. The valid pin combinations are detailed in the SysConfig-PinMux tool.