SBOS558D April 2011 – April 2025 INA200-Q1 , INA201-Q1 , INA202-Q1
PRODUCTION DATA
Although not designed for accurate operation in either of these regions, the INA20x-Q1 family of devices may have exposure to these conditions in some applications. For example, when monitoring power supplies being switched on and off with VS still applied to the INA20x-Q1, it is important to know what the device behavior is in these regions.
As VSENSE approaches 0 mV, in these VCM regions, the device output accuracy degrades. A larger-than-normal offset can appear at the current shunt monitor output with a typical maximum value of VOUT = 300 mV for VSENSE = 0 mV. As VSENSE approaches 20 mV, VOUT returns to the expected output value with accuracy, as specified in the Electrical Characteristics: Current-Shunt Monitor. Figure 9-3 illustrates this effect using the INA202-Q1 (gain = 100).
Figure 9-3 Example for Low VSENSE Cases 1 and 3 (INA202-Q1, Gain = 100)