SLOS224J July 1999 – February 2024 THS4031 , THS4032
PRODUCTION DATA
The input signal source must be a low-noise, low-distortion source with low source resistance. As discussed in the earlier section, the rouse resistance also must be small to avoid impacting settling time. If the source is not a low-noise and low-distortion source, a passive band-pass filter can be added to improve the signal quality as shown in Figure 7-4.