SLOS970B January 2018 – January 2025 TPA6404-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
In addition to the global OTW, each channel also has an individual over temperature warning and shutdown. If a channel exceeds the OTW(i) threshold, the warning register bit is set as the WARN pin is asserted unless the mask bit has been set to disable reporting. If the channel temperature exceeds the OTSD(i) threshold, then that channel goes to the Hi-Z state until the temperature drops below the OTW(i) threshold at which point the channel changes state as indicated by the state control register.