JAJSQ30 june 2023 BQ79616
PRODUCTION DATA
Address | 0x0787 | |||||||
Read Only | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
Name | RSVD | RC_IERR | RC_TXDIS | RC_SOF | RC_BYTE _ERR | RC_UNEXP | RC_CRC | |
Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
RSVD = | Reserved | |||||||
RC_IERR = | Detected initialization byte error in the received command frame. This may due to improper formatting of a byte such as a frame initialization byte is expected, but start-of-frame (SOF) bit is not set, or an invalid frame type is selected. Because bytes received on the COMH/COML are propagated up the stack, it is likely devices in the upper stack will also detect this error. All bytes that follow are ignored until a SOF bit is received. When a communication frame is ignored, the device will not attempt to detect any communication error in the ignored frame nor counting it as valid/discard in the frame counters. 0 = Error not detected 1 = Error detected | |||||||
RC_TXDIS = | Valid when [DIR_SEL] = 0. Device detects the COML TX is disabled but the device receives a command to read data (that is, to transmit data out). The command frame will be counted as a discarded frame. 0 = No error 1 = Error detected | |||||||
RC_SOF = | Valid when [DIR_SEL] = 0. Detects a start-of-frame (SOF) error on COML. The SOF bit is set only in the initialization frame but the SOF bit is set in the current frame that is not expected. 0 = No error 1 = Error detected | |||||||
RC_BYTE_ERR = | Valid when [DIR_SEL] = 0. Detected any byte error, other than the error in the initialization byte, in the received command frame. This error can trigger one or more error bits set in the DEBUG_COMML_BIT register. 0 = No error 1 = Error detected | |||||||
RC_UNEXP = | If [DIR_SEL] = 1, but device received command frame from COML which is an invalid condition and device will set this error bit. 0 = No error 1 = Error detected | |||||||
RC_CRC = | Indicates a CRC error that resulted in one or more COML command frames being discarded. Any other errors in the frame are not indicated as the frame was discarded. 0 = No error 1 = Error detected |