JAJSP34G October 2011 – September 2022 TPS40422
PRODUCTION DATA
The RESTORE_USER_ALL command restores all of the storable register settings from EEPROM memory.
This command should not be used while the device is actively switching. If this is done, the device stops switching the output drivers and the output voltage drops. Depending on loading conditions, the output voltage could reach an undervoltage level and trigger an undervoltage fault response if programmed to do so. The command can be used while the device is switching, but it is not recommended as it results in a restart that could disrupt power sequencing requirements in more complex systems. It is strongly recommended that the device be stopped before issuing this command.