SBAA532A February 2022 – March 2024 ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112C14 , ADS112S14 , ADS112U04 , ADS1130 , ADS1131 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1219 , ADS1220 , ADS122C04 , ADS122C14 , ADS122S14 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS130E08 , ADS131A02 , ADS131A04 , ADS131E04 , ADS131E06 , ADS131E08 , ADS131E08S , ADS131M02 , ADS131M03 , ADS131M04 , ADS131M06 , ADS131M08
Typically, the desired output common-mode voltage of the bridge is at the midpoint of the ADC supply, AVDD, when AVDD = VEXCITATION. This is the ideal common-mode input voltage for an ADC and enables the maximum gain.
Some systems use a VEXCITATION that is greater than AVDD. If this is the case, the bridge output common-mode voltage may not match the ADC input common-mode range. For example, choosing VEXCITATION = 10 V to maximize the sensor output sets the bridge common-mode voltage at 5 V. If AVDD = 5 V for the ADC, then this measurement may be very close to the ADC input range limit. Moreover, high-gain amplifiers used to amplify the bridge output typically limit the common-mode input range to well below AVDD, requiring alternative solutions. Section 6.3 and Section 6.4 show circuits that accommodate bridge configurations where VEXCITATION > AVDD.