The following instructions are a step-by-step
guide to connecting the ADS9110EVM-PDK to the computer and evaluating the
performance of the ADS9110:
- Connect the ADS9110EVM to the PHI. Install the two screws
as indicated in Figure 6-1.
- Use the provided USB cable to connect the PHI to the computer.
- LED D5 on the PHI lights up, indicating that the PHI is powered
up.
- LEDs D1 and D2 on the PHI start blinking to indicate that the PHI
is booted up and communicating with the PC. The resulting LED indicators are shown in Figure 6-1.
- Launch the ADS9110EVM GUI software.