SBAU249A October 2015 – July 2025 ADS9110
Figure 2-1 shows the signal path for the differential signal applied at the board inputs. The board input impedance is 1kΩ with 10nF differential filtering that keeps noise in external cabling common. The overall signal path bandwidth is limited to 160kHz by the anti-aliasing filter formed from a 1kΩ resistor and 1nF capacitor at the amplifier feedback. Finally, the two OPA625 operational amplifiers drive the ADS9110 differential inputs with 2.2Ω impedance up to 7MHz that properly drives the low dynamic impedance of the ADC inputs at 2-MSPS.
Figure 2-1 OPA625 Differential Input Driving Path