The following instructions are a step-by-step guide to connecting the ADS9224REVM-PDK to the computer and evaluating the performance of the ADS9224R:
- Connect the ADS9224REVM to the PHI, and install the two screws, as indicated in Figure 6-1.
- Use the provided USB cable to connect the PHI to the computer.
- LED D5 on the PHI lights up, indicating that the PHI is powered up.
- LEDs D1 and D2 on the PHI start blinking to indicate that the PHI is booted up and communicating with the PC.
- Double-click on the ADS92x4R EVM.exe, file to launch the ADS9224REVM-PDK GUI software. Figure 6-2 shows the ADS9224REVM software folder.