SDAA104 September 2025 F29H850TU , F29H859TU-Q1
To make error debugging easier, error handling functions are integrated in the Code Composer Studio (CCS) as shown in Figure 4-2.
Using CCS Scripts Menu, user can find the error status captured. All the below steps mentioned below for error debug are done with the Error_Agg_Check_Status() hotmenu function in the GEL file executable from the Scripts Menu as shown in the image Figure 4-2.
Figure 4-2 Error Aggregator GEL File
Function