SDAA104 September 2025 F29H850TU , F29H859TU-Q1
The Figure 2-1 shows at a high level how the error handling is done. Error is detected at source which can be a peripheral, module, memory, interconnect or processing unit and this propagates to EAM for error aggregation and then passed on to ESM for user configurable error response within the device. Critical device error events that need error aggregation and logging go through EAM whereas all other device error events are passed on directly from the error source to ESM and are listed in the Error Events table in the ESM Chapter in F29x Technical Reference Manual.
Figure 2-1 Device Error Handling
Architecture