SDAA104 September 2025 F29H850TU , F29H859TU-Q1
Error aggregator module (EAM) is an interface between ESM and critical modules that generate errors like C29x CPU, PIPE, RTDMA, Memory controllers, Peripheral bridges and Read Interfaces. EAM provides error logging and aggregation that is necessary for similar type of errors to reduce the number of errors passed to ESM.
The device contains below EAM module's (where x is from 1 to 3 and y is from 1 to 2) :
For detailed view of the EAM modules refer to the Error Aggregator chapter in F29x Technical Reference Manual.
The following sections showcases error aggregation, error logging and interpretation of the error flag registers with an example.