SDAA516 August 2026 AM620-Q1 , AM623 , AM625-Q1 , AM62A1-Q1 , AM62A3-Q1 , AM62A7-Q1 , AM62D-Q1 , AM62L , AM62P-Q1 , DRA821U-Q1 , DRA829V-Q1 , TDA4AEN-Q1 , TDA4AH-Q1 , TDA4AL-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VE-Q1 , TDA4VEN-Q1 , TDA4VH-Q1 , TDA4VL-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
In the investigated platform, a software mitigation was implemented by standardizing Flash read operations using command 0x6C together with a 4-byte address phase.
Unlike Boot ROM command 0x6B, command 0x6C can operate correctly regardless of whether the Flash device is currently in 3-byte or 4-byte addressing mode, provided the target address remains within the lower Flash address space.
This approach eliminates dependency on the current Flash addressing state during normal software operation. No start-up failures were observed after implementing this modification during repeated MCU_PORz reset testing.