SFFS624B March 2024 – August 2025 MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The UART can be placed into an internal loopback mode for diagnostic, or debug work, by setting the LBE bit in the UART.CTL0 register. In loopback mode, data transmitted on the TXD output is received on the RXD input. Data received on the RXD IO pin is ignored when loopback is enabled. A timer can be used to check if the communication completed within the expected amount of time.