SFFS624B March 2024 – August 2025 MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The IOMUX manages the selection of the peripheral function used on a digital I/O. The IOMUX also provides the controls for the output driver, input path, and the wake-up logic for wakeup from SHUTDOWN mode.
The following tests must be applied for the targeted ASIL as functional safety mechanisms for this module (to provide diagnostic coverage on a specific function):
| Safety Mechanism | Description | Faults | Failure Modes |
|---|---|---|
| GPIO1 | Online monitoring using I/O loopback | This tests the functioning of GPIO. This test also provides coverage for the faults in the IOMUX logic and the I/O drivers. |
| IOMUX1 | Periodic software read back of static configuration registers | Targets the static configuration registers in IOMUX. |
| IOMUX2 | IOMUX coverage as part of other IP safety mechanisms | In general, any fault in IOMUX is covered by the safety mechanisms of the IPs. |