SFFS624B March 2024 – August 2025 MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
In this test method, the GPIO pin is setup with a known value and the status of the pin can be read back using the DIN register. The loopback happens at the I/O driver, and hence, can read the pin status. This method can be applied when the GPIO is configured as an output.