Hall Invalid fault is triggered if the
FOC application detects an invalid Hall State such as 0 or
7. This fault is reported through the Fault status Lock fault.
In case of Hall Invalid fault follow
below steps to root cause the issue.
- Make sure the Hall pin
connections are pulled up at least to 3.3V and check the pin values are toggling
as you rotate the motor shaft manually.
- Check the GPIO's connected to the
Hall pins are configured appropriately in the SYCONFIG.
- Check the variation of the GPIO
pin values in the register view in CCS debug window as you manually rotate the
shaft.