SLUSFQ8B December 2024 – June 2025 BQ2969T
PRODMIX
The UNDERVOLTAGE mode is detected if any of the cell voltage across (V1–VSS), (V2–V1), (V3–V2), or (V4–V3) is below the VUVREG threshold for tUVDELAY time. In this mode, the regulated output is disabled. To return to NORMAL mode, all the cell voltages must be above (VUVREG + VUVHYS) and below VOV.
If the device is used in a system with fewer than 4 cells, Vn pin can be shorted to the (Vn – 1) pin. The device ignores any differential cell voltage below the VUVQUAL threshold for undervoltage detection.
Even when in the UNDERVOLTAGE mode, the device continues to regularly monitor the CTL pin voltage and each cell voltage, checking if CTL falls below VDD–VCTL or if any cell voltage exceeds the VOV threshold. If a condition occurs whereby a cell voltage is above VOV and another cell voltage is below VUVREG, such as can happen in a heavily imbalanced pack, then the OUT pin is activated and the regulator is disabled.