SLUSFQ8B December 2024 – June 2025 BQ2969T
PRODMIX
In the BQ2969T control of the OUT pin can be achieved with external circuitry. The CTL pin can be used as a control input from an external circuit to force the OUT pin to be asserted. OUT Overdrive control is achieved when the CTL pin falls below VDD - VCTL, for the tUVDELAY. This can be achieved with simple circuits, like the N-Channel MOSFET shown in Figure 8-10. The OUT pin remains asserted until the CTL pin voltage rises above the OT voltage trip threshold.
In all operational modes RPD is pulsed at a low duty cycle, making a higher effective resistance of RPD, to avoid drawing significant additional current from the supply.