The device allows a random cell
connection to the VSS, V1, V2, V3, and V4 pins. The device does not require VSS
to connect first and does not require cells connected in a particular order.
However, the OUT pin being temporarily asserted during cell attach is possible,
depending on the timing of the attachment and the external circuitry connected
to the device. The user can want to take measures to check that the OUT pin
assertion at this point does not cause issues on the production line.
If fewer than 4 cells are used,
then short an unused cell input pin Vn to the next lower cell input
pin (Vn-1).
It is recommended to place the
cell input capacitors, supply pin capacitor, and REG output capacitor close to
the device, minimizing trace length on the PCB.