SLUSG35A August 2026 – November 2026 TPS12S24F-Q1
ADVANCE INFORMATION
If the device GND pin connection is lost with MCU ground still connected to ECU ground then device detects loss of ground when device GND voltage exceeds 2V threshold with respect to MCU ground, GATEx drive is disabled regardless of the control signal status in config, active, or limphome mode. If the GATEx drives are already disabled when the ground connection is lost, the GATEx drive remains disabled. During loss of device ground, the total IQ of the device can conduct through any of the following pins: CS, SDI, SCLK, LHI, or DIx/OUT_DISx, using whichever path has the lowest impedance (resistance to current flow) as Figure 7-18 shows.
Table 7-3 lists impact of loss of ground fault on gate drive in different states.
STATE/MODE | GATE DRIVE STATUS AFTER DEVICE GROUND LOSS FAULT |
|---|---|
Low power mode | Bypass FET remains ON and device remains in LPM. Device is capable to detect loadwakeup in loss of device ground fault state also. LPM IQ flows through path shown in below figure. |
Config, active, or limphome mode | GATEx remains off or turns off from on. Active mode IQ flows through path shown in below figure |