SLUSG35A August 2026 – November 2026 TPS12S24F-Q1
ADVANCE INFORMATION
When the external MOSFETs turn-OFF during the conditions such as GATEx control, overcurrent or short-circuit or FET overtemperature protection causing an interruption of the current flow, the input parasitic line inductance generates a positive voltage spike on the input and output parasitic inductance generates a negative voltage spike on the output. The peak amplitude of voltage spikes (transients) depends on the value of inductance in series to the input or output of the device. These transients can exceed the Absolute Maximum Ratings of the device if steps are not taken to address the issue. Typical methods for addressing transients include:
Figure 9-18 shows the circuit implementation with optional protection components.
| COMPONENT DESIGNATOR | DESCRIPTION | RECOMMENDED VALUE |
|---|---|---|
| RVS, CVS | Device gets powered from the VS pin. Voltage at this pin must be maintained above V(VS_PORR) level to provide proper operation during noisy line transients. | 100Ω, 1-10µF |
| RVDD, CVDD | Voltage at this pin must be maintained above V(VDD_PORR) level to provide proper operation during noisy line transients. | 4.7 to 10Ω, 1-10µF |
| CVBBx_BULK |
Need to prevent undervoltage for device during fast output hard-short to ground fault. Place close to device CSx+ pin. |
10-100µF |
| CVBBx_FILTER |
Need to filter out supply transients. Place close to device CSx+ pin. |
0.01-1µF |
| *DVBBx, *DVS, *Q3x, *Q4x |
Needed for input reverse polarity protection |
Schottky diode on VS and VBBx |
| FB1, FB2, CCS, CCSx+, CCSx-, CVIMONx, CTMPx | Ferrite beads (FB1, FB2) can be required at CSx+, CSx- pins for better immunity performance during EMI/EMC testing. Some other filtering is also required based on type of immunity test and frequency band through CCS, CCSx+, CCSx-, CTMPx and CVIMONx to achieve robust immunity performance. Select ferrite beads so that DC Resistance is very low on CSx+ and CSx- pin to avoid significantly impacting ISNS, I2T and SCP accuracy. | MMZ1608B102CTA00, 10pF for CTMPx and 10pF - 100nF for others |
| RGATE_PU, RGATE_PD, DGATEx, RGATEx | Resistors on GATE pins can be used for controlling rise and fall time of external FETs. Separate RGATE_PU must be used for individual external FETs connected in parallel. | Any value |
|
CSRCx, CVOUTx |
Limit slew rate on SRCx pin <200V/us during fast output hard-short to ground fault. Use I = C × dV/dt for CSRCx calculation where I = Peak current, dV is maximum input voltage, dt = turn off time of GATEx |
0.1-10µF |
| RSPI | All SPI or I/O pins
must connect to MCU or other HI/LO source through a resistor for
protection transient events. *Higher series resistor can limit SPI communication frequency so series resistor must be selected carefully based on equivalent parasitic capacitance on SPI lines. |
100 - 500Ω |
|
RSDO |
SDO pin must connect to MCU or other HI/LO source through a resistor for protection transient events. | 100 - 1000Ω |
|
RIO, CIO |
Filters out transient on LHI and DIx/OUT_DISx pins |
0.01 - 10kΩ, 1-10nF |
|
RPU |
Pull up resistor |
1 - 10kΩ |