SLUSG59A February 2026 – November 2026 BQ27Z855
PRODUCTION DATA
The BQ27Z855 device supports charging severely depleted batteries using a zero-volt charge (ZVCHG) or trickle charge feature. To prevent damage to the battery, the device will charge the battery at a very low current level (IZVCHG) when the battery is below the programmable ZVCHG Exit Threshold data flash parameter and a valid input voltage source at PACK+ is present.
Both FETs are disabled while the device is in a ZVCHG state and VBAT is below the POR threshold (VPOR_TH - VPOR_HYS).
For a more detailed description on the BQ27Z855 device's ZVCHG feature, refer to Section 6.3.11.