SLUSG59A February 2026 – November 2026 BQ27Z855
PRODUCTION DATA
The device will automatically terminate charging once the charge current reaches the programmable ITERM value and all Valid Charge Termination conditions stated in the BQ27Z855 Technical Reference Manual are met. After termination, the device operates in Charge Termination mode and disables the CHG FET to disconnect the battery to the system load. The device disables the CHG FET by transitioning the CHG FET to Ideal Diode mode to set CHG = ID_OFF. Power is still provided to the system load as long as the input voltage source is connected.
Termination is only enabled when the CV loop is active and dominant during taper-charge operation. Termination is disabled if the charge current reaches ITERM while the MINSYS loop or battery supplement is active. The device's current limiter will only terminate charging when the current drops to ITERM due to the battery reaching the target CV voltage and not due to charge current limitations imposed by the previously mentioned control loops.
After termination, the CHG FET is disabled and the battery voltage is monitored to check if it has dropped to the programmable Recharge Voltage (VRCH) threshold. If it does, a new charge cycle is established. The safety timers are reset. During charging or even when termination is reached, the device will still support the higher system loads using battery supplement mode.