SLUUCH2 March 2021 BQ40Z50-R2
This command enables/disables the gauging function to ease testing during manufacturing. The initial setting is loaded from Mfg Status Init[GAUGE_EN]. If the ManufacturingStatus()[GAUGE_EN] = 0, sending this command enables gauging and the ManufacturingStatus()[GAUGE_EN] = 1 and vice versa.
In UNSEALED mode, the ManufacturingStatus()[GAUGE_EN] status is copied to Mfg Status Init[GAUGE_EN] when the command is received by the gauge. The BQ40Z50-R4 device remains on its latest gauging status prior to a reset.