SLVSGZ9A February 2025 – May 2025 TPS4141-Q1
ADVANCE INFORMATION
The TPS4141-Q1 measures the voltage on HV (VHV) relative to the voltage on REF (VREF). For bi-directional operation, REF is set to a positive voltage relative to HVGND in the application. The resulting voltage on AOUT (VAOUT) swings above and below VREF for positive and negative VHV, respectively. For uni-directional operation, VREF = VHVGND = 0V or is connected internally to HVGND automatically based on the DIV0 and DIV1 selections. Only positive VHV voltages can be measured and resulting VAOUT is positive with respect to HVGND.
Figure 6-6 shows the transfer function of the TPS4141-Q1 in uni-directional and bi-directional modes. Gain error causes an increase or decrease in the slope of the ideal transfer function curves.
Figure 6-7 shows the transfer function zoomed in of the TPS4141-Q1 in uni-directional and bi-directional modes. Offset error causes a shift up or down of the ideal transfer curves.
There are several error sources that contribute to the overall measurement error of the system. These include, but are not limited, to the following:
Assuming no error sources, Equation 1 can be used to estimate the AOUT voltage (VAOUT_IDEAL):
When including the above listed error sources, Equation 2 can be used to estimate the AOUT voltage (VAOUT) for VREF, VHV, and DIVNOM values of interest:
Assuming no reference error, (REFACC = 0), Equation 2 reduces to Equation 3:
Re-arranging Equation 3, VHV can be computed for a given VAOUT using Equation 4:
The relative percentage error to the ideal transfer curve, %ERRORREL, for a given VREF can be found using Equation 5:
Using Equation 3 and Equation 1, %ERRORREL results in Equation 6: