SLVSIO8 September 2026 TPS638221
PRODMIX
The input voltage of the VIN pin is continuously monitored if the device is not in shutdown mode. UVLO only stops or starts the converter operation. UVLO avoids a brownout of the device during device operation. In case the supply voltage on the VIN pin is lower than the negative-going threshold of UVLO, the converter stops its operation. If the supply voltage on the VIN pin recovers to be higher than the UVLO rising threshold, the converter returns to operation.