SLVSIO8 September 2026 TPS638221
PRODMIX
The device has a power-good function which indicates if the output of the DC/DC converter is in regulation or not. The device detects a power-good condition when the output voltage is greater than 95% of its nominal value and detects a power-not-good condition when the output voltage is less than 90% of its nominal value.
When a power-not-good condition occurs, the device sets the PG pin to logic low.
The PG signal is valid after a delay of 250µs (typ), when the voltage at the VIN pin is above the UVLO rising and the EN pin is pulled logic high, and the device remains active.