SNAA427 October 2025 HDC1010 , HDC1080 , HDC2010 , HDC2021 , HDC2022 , HDC2080 , HDC3020 , HDC3020-Q1 , HDC3021 , HDC3021-Q1 , HDC3022 , HDC3022-Q1 , HDC3120 , HDC3120-Q1
Before attempting to diagnose or improve the RH accuracy of a sensor, it is essential to first confirm that an actual RH accuracy issue exists. While this document focuses on systemic and environmental factors that affect RH accuracy, these initial verification steps are critical to rule out basic functional or setup issues. These verification steps can save users time by identifying that the issue was not humidity accuracy but something else.