This application note concludes with
an appendix presenting three case studies that demonstrate how the outlined
principles can be applied in practice. Each example begins with an RH accuracy issue
of unknown origin. Through systematic analysis using the methods described in this
guide, the root cause was identified and addressed. The selected case studies
represent a range of complexities to highlight that while some RH accuracy issues
are simply resolved, others require more extensive investigation and design
modifications.
- Case Study 1: A user
observed a consistent positive RH offset of approximately 3.5% RH, pushing the
sensor outside of datasheet limits. The issue was later isolated to parts
sourced from a specific PCB manufacturer. Root cause analysis pointed to the
assembly process, due to sensor storage conditions at that facility. The
affected sensors were successfully recovered through a controlled baking
procedure, restoring them to datasheet specifications.
- Case Study 2: In an
outdoor installation, users found that RH sensors initially performed as
expected, but over time were unable to report 100% RH during high-humidity
conditions. The maximum reported RH gradually declined, suggesting a degradation
in sensor performance due to prolonged exposure to saturated environments.
- Case Study 3: In a gas
sensing application, a customer tested two RH sensor products (HDC2021 and
HDC3021) on an old PCB design and a new PCB design. The HDC2021 reported correct
RH results, while the HDC3021 reported incorrect RH results. Investigation
revealed that both chemical contamination and PCB layout errors contributed to
the issues affecting all parts, with opposing effects masking the full extent of
the RH error in the sensors.