SNAS512K September 2011 – October 2025 LMK00301
PRODUCTION DATA
The LMK00301 has an integrated crystal oscillator circuit that supports a fundamental mode, AT-cut crystal. Figure 9-5 shows the crystal interface.
Figure 9-5 Crystal InterfaceThe load capacitance (CL) is specific to the crystal, but typically on the order of 18pF to 20pF. While CL is specified for the crystal, the OSCin input capacitance (CIN = 4pF typical) of the device and PCB stray capacitance (CSTRAY approximately 1pF to 3pF) can affect the discrete load capacitor values, C1 and C2.
For the parallel resonant circuit, the discrete capacitor values can be calculated as follows:
Typically, C1 = C2 for optimum symmetry, so Equation 2 can be rewritten in terms of C1 only:
Finally, solve for C1:
Electrical Characteristics provides crystal interface specifications with conditions that verify start-up of the crystal, but the electrical characteristics do not specify crystal power dissipation. The designer needs to verify the crystal power dissipation does not exceed the maximum drive level specified by the crystal manufacturer. Overdriving the crystal can cause premature aging, frequency shift, and eventual failure. Drive level must be held at a sufficient level necessary to start-up and maintain steady-state operation.
The power dissipated in the crystal, PXTAL, can be computed by:
where
IRMS can be measured using a current probe (for example, Tektronix CT-6 or equivalent) placed on the leg of the crystal connected to OSCout with the oscillation circuit active.
As shown in Figure 9-5, an external resistor, RLIM, can be used to limit the crystal drive level, if necessary. If the power dissipated in the selected crystal is higher than the drive level specified for the crystal with RLIM shorted, then a larger resistor value is mandatory to avoid overdriving the crystal. However, if the power dissipated in the crystal is less than the drive level with RLIM shorted, then a zero value for RLIM can be used. As a starting point, a suggested value for RLIM is 1.5kΩ.