SNAU318 June 2025 LMX1205
The LMX1205 contains a cascaded topology and facilitates the ability to adjust different multiply and divider values for custom frequencies within required operating frequency ranges.
Use the following steps to set the LMX1205 to divider mode:
Figure 4-4 Software Configuration for
Divider ModeUse the following steps to set the LMX1205 to multiplier mode:
Figure 4-5 Software Configuration for
Multiplier ModeIn Figure 4-6, the primary device is set in multiplier mode (× 8), the secondary device is set in divider mode (÷ 4), and the reference clock to primary is 1GHz.
Figure 4-6 Phase Noise Plots for
Multiplier Mode (× 8), 1GHz Reference, and (÷ 4) Divider ModeIn Figure 4-7, the primary device is set in divider mode (÷ 3), the secondary device is set in multiplier mode (× 7), and the reference clock to primary is 3GHz.
Figure 4-7 Phase Noise Plots for
Reference at 3GHz, (÷ 3) Divider mode, and Multiplier Mode (× 7)Figure 4-6 and Figure 4-7 demonstrate that the LMX1205 synthesizes any frequency in a cascaded clock tree using multiplier and divider modes. The LMX1205 complies with the operating range of frequencies for the device.