SNLA239D May 2021 – April 2025 DP83867CR , DP83867CS , DP83867E , DP83867IR , DP83867IS , DP83869HM
Purpose: To make sure that the Common-Mode Voltage is within the specified bounds.
Pass Condition: The magnitude of the Common-Mode Voltage needs to be within 50 mVpp.
Specific Test Setup: Verify the correct test fixture connections. Configure PHY to output Test Mode 4 by setting MDIO registers according to 1000 Base Test Mode 4 in Appendix B.
Connect the DUT ground to test fixture ground for proper measurements (as outlined in IEEE 802.3 in Figure 2-8).
Figure 2-8 IEEE Defined CM Voltage Test Setup