SNLA452 August   2025 DP83TD510E

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Troubleshooting the Application
    1. 2.1 Schematic and Layout Checklist
    2. 2.2 Component Checklist
    3. 2.3 Device Health Checks
      1. 2.3.1 Check Voltage Supply Pins
      2. 2.3.2 Probe the RST_N Pin
      3. 2.3.3 Probe the CLKOUT Pin
      4. 2.3.4 Probe the SMI Pins
    4. 2.4 Read and Check Register Values
    5. 2.5 Verifying Strap Configuration
    6. 2.6 Loopbacks
    7. 2.7 MDI Health Checks
      1. 2.7.1 Link Up Common Issues
      2. 2.7.2 Transmit Level
        1. 2.7.2.1 Change Transmit Level
      3. 2.7.3 Time-Domain Reflectometry
      4. 2.7.4 Signal Quality Check
      5. 2.7.5 MDI Test Modes
    8. 2.8 MII Health Checks
      1. 2.8.1 RGMII
      2. 2.8.2 RMII
      3. 2.8.3 MII
  6. 3Summary
  7. 4References

Schematic and Layout Checklist

When reviewing the schematic and layout, make sure that the design follows the recommended reference guidelines listed in the Schematic and Layout Checklists respectively. This is important to verify various design choices that, if not adhering to the listed requirements, can result in unusual PHY Behavior. This careful review can help in identifying potential design issues early reducing the likelihood of performance problems down the line. Reference and verify all of the noted schematic and layout recommendations in the following checklists:

Industrial PHY Layout Checklist

DP83TD510E Schematic Checklist

The following sections can present expected behaviors if the PHY is powered and initialized correctly. Any deviations from expected behaviors can point to errors due to incorrect peripheral circuitry.