SNLA452 August 2025 DP83TD510E
The following sections approach debugging the application from a high level, starting with application characteristics that have a broad impact before zeroing in on more focused aspects of the design.
This application note is laid out in three major sections:
Depending on the particular behavior observed, all three of these sections are possibly not needed. Because of this, certain sections can be skipped if the correct behavior is observed. The comment is mentioned at the start of each section, as well as given in the following.
Device Health Checks section can be skipped if the device
MDI Health Checks section can be skipped if the device
There are several register settings discussed in this app note. For ease of access, we have included some debug scripts in this application note. These can be used with the tool USB-2-MDIO to reprogram the DP83TD510E into different modes. A collection of all the scripts mentioned here, and more, can also be found on the product page.