SNOU216 February 2025
The software example is created for the LAUNCHXL-F280039C using headers J1/J3 and J2/J4. Ensure the EVM board is connected to the LAUNCHXL-F280039C as BOOSTXL-LMG2100-MD Board (Green) Installed on BOOSTXL Control Board (Red) shows.
Be sure to install Texas Instrument's C2000WARE_MotorControl_SDK V5.02.00.00 or newer software package in the default install path, for example C:\ti\c2000\C2000WARE_MotorControl_SDK_5_02_00.
Follow the steps in Section 3.2 to create an universal motor control project to evaluate BOOSTXL-LMG2100-MD. Please make sure to make the software changes in Section 3.3 so that the software can be used with BOOSTXL-LMG2100-MD.