SPRACF2A April   2018  – January 2026 AM2434 , AM3351 , AM3352 , AM3354 , AM3356 , AM3357 , AM3358 , AM3359 , AM4372 , AM4376 , AM4377 , AM4378 , AM4379 , AM5706 , AM5708 , AM5716 , AM5718 , AM5726 , AM5728 , AM5729 , AM5746 , AM5748 , AM5749 , AM6442

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Ethernet Redundancy in Smart Grid Substations
    1. 1.1 High Availability Seamless Redundancy (HSR)
    2. 1.2 Parallel Redundancy Protocol (PRP)
  5. 2HSR/PRP Implementation in Sitara Processors
    1. 2.1 PRU_ICSSG Overview
    2. 2.2 PRU_ICSSG HSR/PRP Architecture
    3. 2.3 PRU_ICSSG HSR/PRP Features
    4. 2.4 PRU_ICSSG HSR/PRP Firmware
    5. 2.5 Benefits of PRU_ICSSG HSR/PRP
    6. 2.6 Linux HSR/PRP Solution
    7. 2.7 RTOS HSR/PRP Solution
  6. 3HSR/PRP SDK Support
  7. 4Summary
  8. 5References
  9. 6Revision History

RTOS HSR/PRP Solution

The Industrial Communications SDK for AM64x and the Industrial Communications SDK for AM243x features HSR and PRP support using RTOS. The Industrial Communications SDK packages are a single scalable software platform for Industrial Protocols and Drives designs that offers streamlined development across different TI Processors and MCUs. This package provides fundamental software for development of various HSR/PRP solutions. The packages also include sample demo applications that showcase the ability of the software/hardware to implement 1G HSR/PRP. For the Industrial Communications SDK to run effectively, the required MCU+ SDK package would need to be installed. Please see 1G HSR and 1G PRP for a quick start guide on how to test HSR and PRP with the Industrial Communications SDK.

Figure 2-6 shows how the SDK provided RTOS solution addresses offloading HSR/PRP functions to the PRU_ICSSG firmware. Please note that "Hardware Non-offload HSR" on the current SDK provided RTOS solution means that the HSR/PRP feature is completely disabled and there is no concept of running HSR/PRP directly on the R-cores. This is why the figure for "Hardware Non-offload HSR" does not show where the tagging, tag removal, packet duplication, duplicate discard is done. However, experienced RTOS developers are welcome to implement their own HSR/PRP stack to run on the R-cores.

 RTOS Hardware Offload HSR/PRP
                    Block Diagram Figure 2-6 RTOS Hardware Offload HSR/PRP Block Diagram