SPRAD58B September   2022  – February 2026 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , UCC14130-Q1 , UCC14131-Q1 , UCC14140-Q1 , UCC14141-Q1 , UCC14240-Q1 , UCC14241-Q1 , UCC14340-Q1 , UCC14341-Q1 , UCC15240-Q1 , UCC15241-Q1 , UCC5870-Q1 , UCC5871-Q1 , UCC5880-Q1 , UCC5881-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Architectures and Trends
    1. 2.1 Two-Level and Three-Level Inverters
    2. 2.2 E-Axles and X-in-1 Architecture
    3. 2.3 Other Trends in Traction Inverter Design
  6. 3 Key Technology to Enable Traction Inverters
  7. 4 Microcontroller and Power Management IC
    1. 4.1 C2000™ Family
    2. 4.2 Power Management IC
  8. 5 Isolated Gate Drivers
  9. 6 Low Voltage Isolated Bias Supply
  10. 7 High Voltage Isolated Bias Supply
  11. 8 DC Link Active Discharge
  12. 9 Motor Position Sensing
  13. 10Isolated Voltage and Current Sensing
    1. 10.1 Isolated Current Sensing
    2. 10.2 Isolated Voltage Sensing
  14. 11System Engineering and Reference Designs
  15. 12Conclusion
  16. 13References

DC Link Active Discharge

Every EV traction inverter requires a DC link active discharge as a safety-critical function. The discharge circuit is required to discharge the energy in the DC link capacitor under the following conditions and requirements:

  • In an emergency situation or during repairs, the voltage in the system must be safe to touch in less than 2-5s. The emergency situation response must run without an MCU and locally, for example, inside the traction inverter.
  • At vehicle key-off, where all systems remain operational, the discharge happens within minutes.
  • System-level safety requirements of ASIL D

TI has several active discharge designs targeted for different system-level requirements. In general, the active discharge dissipation method can be separated into three categories; resistive discharge, discharge through the power stages, or discharge through the motor windings.

In resistive discharge, a bleeding resistor can potentially work but draws current at all times and is potentially too slow. Therefore, a switched resistor can be used. Using a switched resistor, both ON or OFF control and PWM switching control, can be realized as:

  • Power transistor on or off control using the TPSI3100-Q1 device. The TPSI3100-Q1 reinforced isolated switch driver has an integrated 17V gate supply that can drive the discharge power switches without requiring a secondary bias supply, as the device integrates a secondary bias supply from power received on the primary bias supply. When combined with an external power switch, the device forms a complete isolated solid-state relay configuration. Internal, dual, high-speed comparators enable a communication back-channel with multiple diagnostic features.
  • Controlled PWM using the AFE539F1-Q1 device. The AFE539F1-Q1 smart AFE device has built-in non-volatile memory for PWM and custom waveform generators. The device has added programming ability and logic to enable operation without an MCU. Figure 8-1 shows a scope shot of a DC link discharge using the AFE539F1-Q1 device. Channel 1 (yellow) is the AFE359F1-Q1 output, channel 2 (pink) shows the voltage drop from 950V to 0V. Channel 3 (blue) shows the EN signal input at the gate driver, which initiates active discharge, and channel 4 (green) is the SiC FET drain-to-source current.
AM2634-Q1, C2000, UCC14240-Q1, UCC5870-Q1 DC Link Active Discharge Based on the Smart AFE (Left) and Testing Waveforms (Right)Figure 8-1 DC Link Active Discharge Based on the Smart AFE (Left) and Testing Waveforms (Right)

Energy can be discharged through the motor windings. Dividing a winding-based discharge into multiple stages is possible. These stages include a rapid discharge stage or a bus voltage regulation stage. Generating large negative d-axis current quickly reduces the DC link energy, while the q-axis current must be at zero. Fast loop control from TI’s Sitara™ or C2000™ MCUs and safety isolated gate driver include serial peripheral interface (SPI) programming ability, while six ADC channels provide a reliable and smoothly controlled discharge. Although this design is potentially cost-efficient, the design requires a fully functional system, from the MCU to the bias supply and gate drivers.

A coming trend in traction inverter designs is discharge through the power stages. Here, a pulsed operation mode of the power stages enables discharge through the linear region of the MOSFET, where the MOSFET behaves as a resistor. For this to work, the gate driver requires very precise gate control and a high frequency pulsed operation to not overstress the MOSFET. Alternatively, the gate driver can drive a pulsed short circuit operation mode to discharge a DC link voltage.