SPRADE8B November   2023  – August 2025 F28377D-SEP , F29H850DM , F29H850DU , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P580DM , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Difference Between EEPROM and On-Chip Flash
  6. 3 Overview
    1. 3.1 Basic Concept
    2. 3.2 Single-Unit Method
    3. 3.3 Ping-Pong Method
    4. 3.4 Creating EEPROM Sections (Pages) and Page Identification
  7. 4 Software Description
  8. 5 Ping-Pong Emulation
    1. 5.1 User-Configuration
      1. 5.1.1 EEPROM_PingPong_Config.h
      2. 5.1.2 F28P65x_EEPROM_PingPong.c
    2. 5.2 Testing Example
  9. 6 EEPROM Functions
    1. 6.1  EEPROM_Config_Check
    2. 6.2  Configure_Protection_Masks
    3. 6.3  EEPROM_Write
    4. 6.4  EEPROM_Read
    5. 6.5  EEPROM_Erase
      1. 6.5.1 Erase_Bank
    6. 6.6  EEPROM_GetValidBank
    7. 6.7  EEPROM_UpdateBankStatus
    8. 6.8  EEPROM_UpdatePageStatus
    9. 6.9  EEPROM_UpdatePageData
    10. 6.10 EEPROM_Get_64_Bit_Data_Address
    11. 6.11 EEPROM_Program_64_Bits
    12. 6.12 EEPROM_CheckStatus
    13. 6.13 ClearFSMStatus
  10. 7 Single-Unit Emulation
    1. 7.1 User-Configuration
      1. 7.1.1 EEPROM_Config.h
      2. 7.1.2 F28P65x_EEPROM.c
    2. 7.2 EEPROM Functions
      1. 7.2.1  EEPROM_Config_Check
      2. 7.2.2  Configure_Protection_Masks
      3. 7.2.3  EEPROM_Write
      4. 7.2.4  EEPROM_Read
      5. 7.2.5  EEPROM_Erase
      6. 7.2.6  EEPROM_GetValidBank
      7. 7.2.7  EEPROM_Get_64_Bit_Data_Address
      8. 7.2.8  EEPROM_UpdateBankStatus
      9. 7.2.9  EEPROM_UpdatePageStatus
      10. 7.2.10 EEPROM_UpdatePageData
      11. 7.2.11 EEPROM_Get_64_Bit_Data_Address
      12. 7.2.12 EEPROM_Program_64_Bits
      13. 7.2.13 EEPROM_CheckStatus
      14. 7.2.14 ClearFSMStatus
    3. 7.3 Testing Example
  11. 8 Application Integration
    1. 8.1 Software Functionality and Flow
  12. 9 Adapting to Other Gen 3 C2000 MCUs
  13. 10Flash API
    1. 10.1 Flash API Checklist
      1. 10.1.1 Flash API Do's and Do Not's
  14. 11Source File Listing
  15. 12Troubleshooting
    1. 12.1 General
  16. 13Conclusion
  17. 14References
  18. 15Revision History

EEPROM_Program_64_Bits

The EEPROM_Program_64_Bits() function provides functionality for programming four 16-bit words to memory. The first parameter, Num_Words, allows the user to specify how many valid words are written. The data words are assigned to the first 4 indexes of the Write_Buffer to be used by the Fapi_issueProgrammingCommand function. If less than four words are specified in the function call, missing words are filled with 0xFFFF. This is done to comply with ECC requirements.

First, a full EEPROM unit is tested for.

EEPROM_Get_64_Bit_Data_Address();

Next, the Write Buffer is filled with 1s if less than 4 words are specified.

int i;
for(i = Num_Words; i < 4; i++)
{
    Write_Buffer[i] = 0xFFFF;
}

Next, data is programmed and the pointer is incremented to the next location to program data.

// Clears status of previous Flash operation
ClearFSMStatus();

Fapi_setupBankSectorEnable(FLASH_WRAPPER_PROGRAM_BASE+FLASH_O_CMDWEPROTA, WE_Protection_A_Mask);
Fapi_setupBankSectorEnable(FLASH_WRAPPER_PROGRAM_BASE+FLASH_O_CMDWEPROTB, WE_Protection_B_Mask);

oReturnCheck = Fapi_issueProgrammingCommand((uint32*) Bank_Pointer,
                                                Write_Buffer, 4, 0, 0,
                                                Fapi_AutoEccGeneration);

// Wait for completion and check for any programming errors
EEPROM_CheckStatus(&oReturnCheck);
Empty_EEPROM = 0;
// Increment to next location
Bank_Pointer += 4;
Note: This function cannot be used until RESET_BANK_POINTER has been executed to set the pointer. In this example, it is called in EEPROM_Config_Check(). Executing before can produce unknown results.