SPRADE8B November 2023 – August 2025 F28377D-SEP , F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Generation 3 C2000 MCUs come with different configurations of Flash memory that is arranged in multiple sectors. Unfortunately, the technology used for the on-chip Flash memory does not allow adding a traditional EEPROM on the chip. Some designers use an external EEPROM part for such non-volatile storage. The good news is that Flash memory is a specific type of EEPROM and all Generation 3 C2000 MCUs have in-circuit programming ability for the Flash memory. This application report makes use of this facility and allows using sectors of on-chip Flash as EEPROM by emulating the EEPROM functionality within the limitations of the Flash memory. Note that at least one Flash sector is entirely used as an emulated EEPROM; therefore, this is not available for the application code.