SPRUJC0A June 2024 – June 2025
The connector J102 is provided to debug an external target with the on-board XDS110 debug probe. This connector allows the LaunchPad to be used as a stand-alone XDS110 debug probe. For mating connector and cable, see Samtec FFSD or equivalent.
If the LaunchPad is being used in this manner, then make sure that all of the jumpers are removed from J101. This isolates the JTAG signals from going to the F28P550SJ9 MCU. UART TX and RX signals from the XDS110 device are also included on this connector.