SPRUJC0A June 2024 – June 2025
The F28P55x LaunchPad has several power domains that can be connected or isolated from each other with removable shunts. The different 3.3V and 5V power domains are further described in Figure 2-2 and Figure 2-3.
Table 2-1 describes the usage of the different removable shunts on the LaunchPad board.
| Shunt Identifier | Usage Description |
|---|---|
| JP1, +5V0 | Connects the +5 V power from the USB-C connector (+5V0_USB) to the +5 V power on the XDS110 side of the board (+5V0_XDS110). Bridges the power and ground isolations between the two board sides. |
| JP1, GND | Connects the board Ground on the isolated USB-C connector side of the board (USB_GND) to the rest of the board ground (GND). Bridges the power and ground isolations between the two board sides. |
| JP2, +5V0 | Connects the +5 V power on the XDS110 side of the board (+5V0_XDS110) to the +5 V power on the F28P55X side of the board (+5V0_MCU). |
| JP2, +3V3 | Connects the +3.3 V power on the XDS110 side of the board (+3V3_XDS110) to the +3.3 V power on the F28P55X side of the board (+3V3_MCU). |