In this reference design, the reference signal for
current and voltage loops uses the DAC70502, 14-bit DAC, which is programmed using
the USB2ANY interface adapter.
Use the following steps for the initial setup of a new USB2ANY device:
- Open the USB2ANY Explorer
- Click and hold the button inside the small hole of the USB2ANY before plugging
the device into the computer
- The software prompts for an update after the device is plugged in
- Confirm the software update
- Release the button
USB2ANY sets up the device properly.
Use the following steps to configure the DAC:
- Open the USB2Any Explorer
- Click the Select Interfaces button. The Select Interfaces window
opens
- Select SPI
- Close the Select Interfaces window
- In the USB2Any Explorer window, select SPI above activity logging.
If the SPI tab is not shown, click around the space above activity
logging because the tabs can be hidden.
- Write data code into the terminal to generate the desired output parameter
Figure 4-2 shows the GUI parameters for the setup.