TIDUFF0 December 2025
The AWR2188, DS90UB971S-Q1 as well as MSPM0G3519-Q1 supports I2C as well as SPI communication. The board also supports both interfaces. By default, I2C is enabled to communicate between the DS90UB971S-Q1 and MSPM0G3519-Q1. The MSPM0G3519-Q1 communicates through SPI to the AWR2188 and through I2C to the PMIC.
The connection scheme can be modified to connect the DS90UB971S-Q1 through SPI to the AWR2188 directly and communicate through I2C to the PMIC. This way the MSPM0G3519-Q1 can be bypassed in case the MCU is not required. Complete the following to implement this change:
Figure 3-2 Schematic of SPI and I2C
Connection